Hi,
So I’ve been looking for a series of resistors that can suffice in the operating conditions that I need to put them in. They’re fairly low current (I’m usually dealing with less than 10 mA), but it’s high voltage (My current design assumes a max of 450 VDC, but I wold like to make it to where I can use this same design, and change a few parts to go to my max theoretical spec of 800V). And I need a wide range of values for resistance (I’m using them for voltage dividers). It doesn’t necessarily have to be from the same series, I just need to know what series that I can go for, because I can’t find them
It’d be especially good if I can find resistors that have values of 10k, 6.98k, and 280k, because that’s currently what I have in my build.
Thank you,
G