Resistor

I’m a little bit confused. I need resistors that are not marked. Reads on the multimeter 0.530 M ohms can you give me an explanation, so that I can make sure I have it right.

I checked in our system and I was able to find one option with this value as part 13-MFR1WSDRD52-530KCT-ND. Unfortunately I am unable to confirm what wattage rating your origional resistor is, do you know if 1W will be enough?

Can you post a photo?

0.53M = 530K so it could be a 500K +/-10% or +/-20% resistor

That appears to be a very old 1% metal film resistor, probably made before 1970. The circuit context appears to be a frequency shaping control of some sort. The size implies >= 0.5W power rating that while way over specced for the apparent application was often the most economical choice 50+ years ago.

Considering all that, I suggest you try out the part that @Rob_Johnson linked above.

Thank you that helps a lot. It’s a very old amplifier

These two big resistors get incredibly hot….what do you have to replace them……

Hello @mikecasey,

Please let us know which resistors you are referring to.

I understand the make and model information has worn off your amplifier. However, a few pictures may help us determiner narrow down the search.

Sincerely,

Aaron

These are the resistors. What does 5PCK mean.

I’m guessing 5watts. But I just want to make sure

mikecasey,

Without knowing the series and manufacture, there is no way to be sure what each number and letter would call out.

Mikecasey,
Part number
4506-HVLR5208F10K0K9-ND is the only 5 watt option I found for 10K ohm 1% film resistor.

Hello @mikecasey,

It looks like the resistor is connected to a rectifier tube (likely a 5U4 or 5R4). If I had to guess, the resistor provides power to the input stage of the amplifier.

  • Yes, the red power resistor will get hot.
  • The red power resistors do not show signs of stress
  • The little resistor in this picture requires attention

The markings for the red power resistor likely indicate a 5 % tolerance.

Recommend you test the resistance using a multimeter. Replace only if significantly out of tolerance.

Happy soldering,

Aaron

I am trying to draw this circuit so I can do more research…..is there enough info here so you can tell me which class of amp this belongs, so that I can narrow down what to look for. Also can you tell what options I have for tubes T5- T8- and T9.
And although I do have volume on channel 1. it is very low. Channel 2 is just dead no sound at all….Also it has a hum. I removed tube 8 and the hum disappeared . If you have the time, I know you’re busy, would you give me your thoughts. Mike


Hello @mikecasey,

This is a classic push-pull 6V6 amplifier with a 1940 to 1960 design.

Unfortunately, I am unable to determine the tube types from you drawing.

Recommend:

  • Purchase “The Tube Amp Book” by Aspen Pittman. This reference is full of schematics for vacuum tube guitar amplifiers.

  • Search Antique Electroncis Supply for New Old Stock (NOS) tubes.

Sincerely,

Aaron