Morning - am looking for current model number of the following schurter switch please
Hello! Looks like that is part number TA45-ABCRLC00E4-AZM01-ND. The model number matches almost perfectly to the marking on your label. The only thing I cant confirm is the “AZM01” suffix on the model we stock, but if it helps that code only calls out mounting specifications, so the actual ratings and performance should be the same.
switch is rated for 120VAC that I want to replace - this appears to be 240VAC
I think this may be best option?
DigiKey Part Number
486-4541-ND
The 4430.2643 @chris_groom had listed looks to be the exact match.
–The 240v it the absolute maximum rating the switching contacts can handle.
The-120vac is apart of the breaker’s trip function.