Looking for replace DMC-1112 switch

Hello, I am looking to replace this switch and having trouble. Can you please let me know what the equivalent would be. I believe it is NC (normally closed).

This is for a Seaflo water pump.
info written the switch:
side one:
defond
15(3)A 250v ~ T85
DMC-1115 (mirco sign) 5E4

side two
12A 12VDC T105
DMC-1112

Thank you,
Ron

Hello Ron,

Thank you for your post.

I am able to narrow down our options to a point, but there are a few things I am not able to determine.

The function appears to be either constant On or Off with a then Momentary function when the button is pressed. You will need to choose that parameter from our filters. Also I could not determine the size of the connection tabs, so you will need to choose that as well.

There is also the amount of operating force to choose. The lower the number the easier to press the button.