A little background: Relay RY701 (in series after C701) is chattering 3-5 times when powered on cold start or after a minute or so after last start. Capacitor C701 VAC readings vary on each pulse as OL and < 50VAC during chatter; then stabilizes at 117VAC and fully powers on. ESR of C701 is OL/OF when measured in circuit and after removal of capacitor.
Pic of C701 attached & the R-117 service manual describes the C701 as:
C701 08E04371SO1 MF 0.01 uF
Appreciate your time and help.
Welcome to the forum.
Given the receivers’ age it’s quite possible that film capacitor is the problem.
Here’s a search giving suitable parts electrically, you’ll need to choose one based on best size fit and price.
Radial Film Capacitors | Electronic Components Distributor DigiKey
Thank you Paul! Looks like the 250VAC selection is limited to a metallized paper cap; would it be ok to bump up to 275VAC? Incoming mains is 117VAC.
Yes, a higher voltage is always better in this type of application.
Thank you…have a great weekend!
Sincerely,
Joe