Microsemi FLASHPRO5 Installation Trouble Shooting

This post may help you if there is a problem when connecting to your Microsemi FLASHPRO5.

When using the FlashPRO5 programmer, you can download and install the latest release of FlashPro or FlashPro Express from the Microsemi website.

There is no other configuration or firmware required. If the power LED is on and you are able to select the device in the FlashPro software, it should be ready to use.

If you encounter a problem starting the device, please study the Software/Hardware Installation Guideline.

You may also need to be aware that errors can occur because there is something interfering with the power rail on the target board, so it could help to measure and double-check the voltage on the Vjtag pin.

To learn more, please refer to our post: No Serial Port Created by Maker Board

FlashPRO5 adapter is not recognized by Libero or FlashPro Express tools. Device manager shows it as 4 COM ports. Make Board is properly recognized as FlashPro5 by those tools. What could be a problem ?

Any solution to this? I have the same issue.

Thanks,
Jon

This 2018 post might help (last post in the thread linked in the OP).