Questions concerning the MTBF specification for aluminum electrolytic capacitors are a common request DigiKey receives from our customers. In short, aluminum electrolytic capacitors are not rated in terms of MTBF. These capacitors contain multiple materials, so they are rated in hours of expected life. Under different conditions the expected life of the part changes. As one example of this, DigiKey supplier Chemi-Con has the following to say about aluminum electrolytic capacitor MTBF.
“For designing the device with aluminum electrolytic capacitors, a failure rate and useful life are necessary to be considered for their reliability. The failure rate of aluminum electrolytic capacitors is approximated by the bathtub curve shown in below figure.”
Source from Aluminum electrolytic capacitor Reliability | Nippon Chemi-Con Corporation
and also lists on the datasheet of ALC10 Series from Kemet:
See also
MTBF, MTTF and FIT Data - Support