I have struggled for hours trying to find a connector that suites my purposes, and have looked on and off for several months. I am trying to find a small edge to edge board connector pair that undergoes multiple disconnects. My first prototype boards used a 1.27mm(0.05in) pitch rectangular right angle pin and socket, very similar to dupont connectors except half the scale. These did not hold up and bent frequently. I need the connector to be small but robust. The boards are going to be coplanar.
The only connector that I have found that sort of work is the Keystone 6100 and 6102 connectors. These are great 10 amp small connectors, but they are effectively 3 mm pitch and individual connectors, not a 4 pin assembly like what I need. I have used the keystone connectors for power, but they are too big for data lines.
I would really appreciate help finding a connector, I would rather order a preexisting connector than have a team design a custom connector. I totally understand if this is not feasible, I have already invested a significant portion of my time looking for connectors with no results. Thank you!