Need help finding amphenol pcb mount connector

I’m in need of a few of these connectors but I can not seem to find it or a suitable replacement. Thank you

Hello hidaudiotech,

Welcome to the DigiKey TechForum.

The main dimension for finding an alternate part, would be the pitch, or pin spacing.

Can you provide the Center-to-Center measurement? With this size of connector, it should be close to 10mm, but clarification would help with finding the options.

Click Here for the options that are 10.00mm and 10.16mm pitch.

11 mm pin spacing thank you.

That is the outside to outside of the pin, and not Center-to-Center.

Got it. Thank you very much!

You’re welcome.

Be sure to check the datasheets, to find ones with 2 pins per wire.

The single pins would work also, but will not be as sturdy on the board.