We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
My Ecobee thermostat is not generating stable 24V control signal, so I took it apart and it appears Q19 is damaged. I would like to replace the part but could not find any information on it. It’s a 2x2mm package, and potentially it’s a MOSFET as a transmission gate to connect an output (Y-wire) to the 24VAC source.
I did a search on the marking information on the part itself and wasn’t able to find much, but do you know what model the ecobee thermostat is? It would be worth a search to try and locate a schematic and in turn a part number from there. Without any other information though, I’m not able to provide a solid list of options.
It is the latest ecobee thermostat (5th gen). I was hoping to find a schematic of any generation of ecobee but had no luck. I wonder if there are measurements to at least identify the functionality so can narrow down the list? Thanks!
If I knew what the package was called I’d be able to narrow it down a lot more as well. I know a lot of these can be ruled out on the package size alone. It’s a bit hard to tell, but does it have only 3 terminations to the board or 6?
The package should be DFN-6 2x2mm. I am not sure if all the leads are wired, but looks like the top two left are shorted internally as they share similar burnt marks. The damage is most likely caused by over current, so I would assume those two leads are source/drain. Is it possible it’s a P + N as a CMOS transmission gate?
It’s hard to know for sure without good documentation… Its even trickier with 6 pins.
Here is an updated link with different variations of the DFN-6 package size. Different manufacturers call them different things so I kept it a bit broad.