Need help in identifying these two capacitors and specs 9518/9544
Thank you!
Hello,
Unfortunately I could not identify these for you.
Thank you for your inquiry.
Visual identifcation of your two parts suggests they are not Capacitors, that you have Crystal Oscillators in an HC-49/US package size.
It’s likely the 4.91 written on the top means 4.91Mhz.
The closest values we have to that are 4.9152Mhz - Click Here
Changing a Crystal from 4.91Mhz to 4.9152MHz may have detrimental effects to the device.
The logo on the parts indicate that they are both NDK parts. Unfortunately, it does not appear that they still make the HC-49/US package that you have.
It’s highly likely that the crystal marked “4.91” is actually 4.9152MHz and is only showing the first few digits for space reasons. That frequency is a very common frequency used in devices which have a UART and/or an RS-232 serial port because it divides down evenly to common baud rates used for such applications, such as 1200bps, 9600bps, 19200bps, etc…
Therefore, the link that @Kristof_2649 gave to the 4.9152MHz crystals is the correct one.