Need some technical clarification on the a product (Digi-Key Part Number "1993-PST360G2-2OO-C0002-E)

I am willing to buy a PST-360 Hall-Effect Through-Shaft Rotary Position Sensor having Digi-Key Part Number “1993-PST360G2-2OO-C0002-ERA360-RE-ND.” According to the specification, it has ERA 360 degrees but in my application, I need to measure -10 deg to +10deg. So can I set the origin between 10 to 350 deg and measure -10 deg to +10 degrees perfectly?

Hello, Sundeepreddy. Welcome to TechForum!

The datasheet for this device, page 2, shows a linearity graph with 10% to 90% range. It states that linearity is only guaranteed within the electrical rotation angle, 15 degrees to 360 degrees. I believe you can likely make this device do what you need as a 20-degree span is within the ERA specification, but you may have to study it further and experiment some to ensure you’re seeing what you need to from the device.

Thank you for your reply,
Our existing communications have a CAN speed of 1MHz. Can you also please confirm what is the CAN speed (Hz) of this device?