Does DigiKey sell a 1-ft USB-A male to USB-A male cable that does not pass power over between USB devices?
Welcome to the TechForum. I am not sure what you mean by pass power. Once they would be plugged in on both sides, they would pass the information . Generally a USB passes data information so there is not a lot of power that should flow through either side. I would not think this would be an issue .
These are close to the size needed:
I am presently using this device on the end of a standard A to A cable. My preference would be to not have to add this device and have an A to A cable that doesn’t have the power pins connected.
I do not see we have anything like this. The cables do not have anything like this on the parts we sell. Thank you for the further explanation. Though this is a public forum so maybe someone else has an idea. I am not the only one that will see this. So hopefully someone will have another suggestion.
Hello @Sk3wMohan ,
Unfortunately the only offering DigiKey currently has would be the parts to build your own cable using only the two center data pins within the USB-A Male connectors like these, click here. This may not be ideal for you, but thought to share in case you cannot find a finished cable elsewhere.
Example cables to use:
Shielded Spiral Multiple Conductor Cables
Other Multiple Conductor Cable Options
Flat Ribbon Cable options 900-1000570226-DS-ND | 1233-969M101-20-2-DS-ND