NTC 10k Probe dimensions: Ø4 × 24 mm

I’m looking to replace a Daiken sensor 129970
I need a NTC 10k Probe dimensions: Ø4 × 24 mm

Hello,

We do not carry this probe.

Unfortunately we cannot filter these parts by the dimensions. Here are what we have for 10K options. You will need to review the datasheets to find the dimensions for each part. If you make use of the other filters available you can narrow down the number of datasheets you will need to look through.

NTC Thermistors | Temperature Sensors | Electronic Components Distributor DigiKey

If its full part number is 129970J, then it appears to be an HVAC part that is fairly easy to source from HVAC parts suppliers.

Example online suppliers (check local suppliers too),

Hi Paul, Can you verify if the Daikin 4026843 sensor has the same values as the 129970J?

As far as I can tell, Daikin Part# 129970J is not the same as Daikin Part# 4026843.

Both items come up in Google search using just Daikin and then the part number.

If its not the same in connector or cable length, I don’t mind, as longas the B-value and working temperature range are the same.