Can the RER190-39/14/2TDLOU fan be turned on and off via the 0-10V control line? That is can it be turned on by applying the fan voltage, e.g. 24 VDC, to the control line to turn it on and removing the voltage to turn it off? The application would be to turn the fan on and off via a thermostat.
Greetings,
The fan in question appears to follow the pattern that is typical for small DC fans, which is discussed at some length in this post.
If simple on/off control is desired, connecting the control lead to ground should turn the fan off, while leaving it unconnected should result in full-speed operation.