Hello, I am looking for a replacement 14-131.012. the product on the website doesn’t indicate if the LED colour is specified and the image photo doesn’t look like it has a lens. So wanting to confirm these things come with the part that I want to order.
Hello OPSGroup,
Welcome to our community and thank you for contacting DigiKey Technical Support.
There appear to be associated products for part number 14-131.012.
The 012 suffix is not listed in the catalog; I am going to contact EAO to ask about the proper associated products.
Hello OPSgroup
EAO has advised part number 14-131.012 (1948-1232-ND) has been phased out.
EAO has offered part number 14-131.022 (1948-1233-ND). Please see page 300 of the catalog below.
EAO_14_Main-Catalogue.pdf (1.9 MB)
The difference between the two parts numbers is the terminals. The part number ending .012 has silver terminals. The part number ending .022 is gold over silver terminals.
You will need to order the following parts,
Front bezel raised design – see catalog page 323
Diffuser/ marking plate– see catalog page 323
Lens – see catalog page – 321
If illumination needed, see catalog page – 325
Hello OPS Group,
Becky provided excellent advice. I just want to add that Digikey has a configurator that can be used to find compatible parts for 14-131.022.
I built the following assembly based on your image, so it may not be correct:
But you can change any of the components by clicking on the pencil icon. When satisfied with the specs, you’ll see the part numbers just under the large font description. Or, you can add the items to a Digikey cart to see them.
I hope this helps. Please let me know if EAO can be of further assistance.
-Jason