Part information

I purchased a

2368-54-718-ND

54-718

SWITCH TOGGLE DPDT 3A 125V

on order #Redacted for safety

on 11/10/23

I want to replace it with a SWITCH TOGGLE DPTT 3A 125V

I want it to look just like my DPDT and fit in the same hole.

I cannot seem to find specs on the DPDD that I have, so am lost trying to search for DPTT

Can you help me?

Hello gappel69 and welcome to the DigiKey TechForum.

From what I could find about 2368-54-718-ND, it appears to have a 13.3mm long actuator and have solder lug termination. Unfortunately, I have been unable to find a panel cutout dimension for this part.
If by DPTT you are meaning you want a Double Pole, Triple Throw. I was able to find the options linked HERE that are the closest to the specifications you listed. They are rated for 5A 120VAC and have a range of actuator lengths from 10.67mm to 17.45mm.
If you mean something different than DPTT, can you please explain.

1 Like

Thank you very much nick_13812.

I think the 7411TZQE is going to do exactly what I want.

Thanks nick_13812
I think the 7411TZQE is going to be just what I need.