Cannot find the right caps on DigiKey. Looking for Rubycon 50v 47uf, 10mm diameter,16mm in-board height, through-hole and Rubycon 50v 100uf, 12mm diameter, 21mm in-board height through-hole capacitors.
For the 47µF cap I found the 1189-2325-ND
For the 100µf cap I found the 1189-1659-1-ND
Hi panegyric13,
We have these in our system:
>=50V 47uF, 10mm diam, 16mm height Rubycon caps (note that we add the datasheet tolerance for maximum possible height in our listings, but these are referred to as 16mm height)
>=50V 100uF, 12.5mm diam, <=21mm height Rubycon caps
What series markings, temperature, and/or life ratings do you need? There might be other options from other quality vendors as well, depending on what you actually need.
These are for a vehicle board…
Automotive option for each.
1189-1009-ND for the 47µf
For the 100µF
P10776-ND but it is not Rubycon though. It is in-stock however.
Additionally We would like to have the lead spacing (center to center) for these too to help look for options that would have a higher chance to hit.
Lead spacing is 5mm for both. I ordered caps with the right specs but they are considerably smaller. The original caps are off an OLD vehicle and maybe the smaller ones will still work?!
Caps I ordered: 1189-50NXA100MEFC10X16-ND and 1189-1649-1-ND
The 1189-50NXA100MEFC10X16-ND is a Bi-Polar Cap the original is polarized. Please replace with a polar type. Here is a suggestion for an Automotive 100uF 50v radial cap with 5mm lead spacing 1189-2311-ND.
1189-1649-1-ND should work.