Hello, welcome to the Techforum!
I was able to find 1189-200TXW220MEFR18X25-ND in our system as a possible match, can you confirm if the length and diameter match your capacitor?
Hi desmetde,
I managed to find an old datasheet of the obsolete Rubycon USR series, which is what you have there. It’s an 85°C 3000 hour part rated for a ripple current of 1.13A at 120Hz. I found a recommendation on their website suggesting the USG series as the replacement.
I also did a search just based on parameters and dimensions and came up with a Rubycon from the USG series, as well as another slightly shorter part from Nichicon. Both are 220uF 85°C 3000 hour 20mm diameter by 25mm height parts.
- Rubycon 250USG220MEFCSN20X25 250V, 1.23A ripple current
- Nichicon LLS2D221MELY 200V, 1.19A ripple current
If you have extra clearance, either in height and/or in diameter, here are some other caps which meet or exceed the ripple current and lifetime/temperature ratings of your part. Take special note of their dimensions to ensure they would fit in your application.
David, i truly appreciate you, wow
please choose the one you feel is best, i do have room on the board and the cabinet for a taller Cap, pick the one you feel is best
Thanks,
Daniel
David, I only need one though, is this ok?
Dan
Hello Dan,
Any of the previously suggested substitutes you can just buy one of. They are in stock and ready to ship.
Ok, how do I order? Pay?
I’m ready to order
Thank you
Daniel
If you are on the page for one that you’re wanting to buy, lets say for example 1189-3886-ND, you can proceed from there by clicking add to cart after putting the desired number of the caps in the quantity section.
And then proceed to check out if that is all you’re buying.
Otherwise if you find that process too bothersome you can call our sales personnel and they will be glad to place an order over the phone for you. The number is 1-800-344-4539.