Parts and Connectors for the Mintron

Hello,

The connector in the forefront from a Mintron Camera has an outside of 2mm * 4mm and is two pin.

The connector near the NTSC sticker is two pinned and 3.40mm * 4.20mm.

I figured one was a UART connection but am clueless so far.

Does your company have connectors of this size and shape that are each two pin types?

Seth

silver2row

Thank you for contacting DigiKey , I have looked through our connector selection and I am not finding these connectors . Is there any markings on the headers that may help us identify them ? What is the pitch of the contacts center to center ?

Thanks Craig

Hello…I will try to figure out the pitch and return service. Thank you.

Seth

3.40mm * 4.20mm = 2mm pins

2mm * 4mm = 1mm pins

For the above dimensions, those are outside dimensions for the square type connectors.

Seth

@Craig_2048 ,

Sir, I think this version and this is an older, unsupported type of non-Open Source hardware/software.

The company, Mintron, does not even list this type of camera under their website online.

I have looked for different types of data relating to the Mintron in question but I have fallen short.

Seth

P.S. The connectors, although older, may have a newer form factor that can be fitted well enough.

If you need the ID of these connectors, please let me know.

Hi silver2row,

Here’s one of them:

10114828-10102LF Amphenol (FCI) Minitek series 1.25mm pitch header
image

Though less certain about the other one, it looks quite a bit like this guy:

BM02B-SRSS-TB JST SH/SR series 1.00mm header
image

Hello @David_1528 , first off.

You rule…

Secondly, are there any connectors (female) that go along with those? I am not sure how you found those connections. Thank you.

Seth

P.S. I will click on the links available that you posted and look for mating connectors.

Hello @silver2row

The mating housing and contacts for part number 10114828-10102LF are;
10114826-00002LF the housing
10114827-001LF the contacts.

The mating housing and contacts for part number BM02B-SRSS-TB are;
SHR-02V-S the housing
SSH-003T-P0.2 the contact

Yes, if you scroll down the page on the links I gave you, the mating connectors are listed. From the mating connector listed, there will be links to the contacts required for them. You’ll note that the crimpers designed for these contacts are seriously pricey.

If possible, I’d recommend using the pre-assembled housings with wires attached. That will save you time and $$$.

Oh, and for the first connector, it looks like Molex makes what appears to be a compatible part in the Picoblade 1.25mm 0533980271.

image

The advantage for this one is that we do have some pre-assembled cable assemblies with the mating connector already attached. Specifically, part number 0151340205.