Hi all,
I would like use one of the components (output as a single output) in this series. So, I have question on page 9 in the datasheet. I would like to have a constant output voltage, so I don’t want the output voltage adjustment either increase or decrease. So, what should I do to keep the output voltage constant?.
Thank you.
pinkyponky, Page 9 of the datasheet says: The output voltage can be adjusted (single outputs only) by using the trim pin and the use of either an external trim pot or the use of a single fixed resistor. If the trim function is not needed, leave the trim pin open.
So if you do not want to adjust the output voltage, do not connect anything to the Trim Pin.
1 Like