I need some soldered pin connectors (or socketed maybe) to connect 2 boards together. The normally connect with DB25 F & M laying end to end. I need to be able to connect these 2 boards in a sandwich configuration. Is there a pre made 25 pin DB25 profile pin part that can be soldered in? If so is there a part#?
Are individual pins available approx. 1.5mm that I can at worse case individually solder in place? Part#?
Then possibly the most convenient but more costly, is there a M/F individual pin set that can be used so the boards can be unplugged if needed?
Hi coinop,
Welcome to the TechForum!
I’m not certain I’m understanding what you are looking for. If I understand what you have now, it’s mating DB25 connectors mounted on the ends of two circuit boards, each in a right angle configuration so the boards mate up end-to-end.
If this is correct, then would two DB25 mating connectors mounted vertically rather than at a right angle be what you need? Here are some examples of such connectors.
Vertical DB25 receptacle
Vertical DB25 plug