Planet IGTP-805AT

Hey!

Kindly provide guidance, I am looking to buying Planet IGTP-805AT. Is it safe and practical to use it in Egypt?
FYI Egypt has a 220V / 50Hz electrical system.

Thank you in advance.

Hi,
Welcome to the Digikey tech forum. I’m not sure if part IGTP-805AT is available in Egypt since it falls under our “Marketplace” product which are typically only available in the US. I also looked at the voltage input for it and you would need to convert it to 12 ~ 24VAC or 48VDC . Take a look at this similar item, Digikey part 95-N785-H01-SFP-ND , the input for this is 100 ~ 240VAC at 50/60Hz and may be a good alternate for your application.

1 Like

Since the product is from a company in Taiwan that does not sell direct they very likely have an authorized distributor/retailer for Egypt. You can ask them directly at their sales contact page.