PLC Teardown: Modular Construction Isolation and Repair

In this post, we peek inside a PLC to better understand why they are described as “hardened” industrial computers. We can see the 32-bit microelectronic electrically cocooned from the hazards of the industrial environment.

A PLC is an armored microcontroller!

PLCs share a modular construction with stacked PCBs (Figure 1):

  • Base: Power / I/O PCB
  • Middle: Logic board with microcontroller and communications interface (e.g., Ethernet)
  • Top: Human-Machine Interface (HMI) with display and pushbuttons

This article is part of the DigiKey Field Guide for Industrial Automation

Location: Understand It → Teardowns
Difficulty: :seedling: Student — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 13 Mar 2026


Figure 1: Image of a PLC with cover removed showing the stacked PCBs.

Modular Construction

Most OEMs produce families of PLCs. They differ in output type (relay vs solid state) and power supply (24 VDC vs 120 VAC). These options are typically incorporated into the base power / I/O board. This allows the OEM to swap the base board as required. As a result, the logic PCB and the case require minimal (or no) modifications. For example, the power board for the Siemens LOGO! shown in Figure 2 has 24 VDC power supply input, 24 VDC inputs, and four output relays.

Figure 2: Image of the PLC circuit boards power / output (left) logic (right) and HMI (middle).

Isolation of the Sensitive Logic

The power / I/O is designed to protect the logic board from hazards of the industrial environment. It’s like a cocoon surrounding the microcontroller. For example, the Texas Instruments Tiva C microcontroller as shown in Figure 3 has a 3.3 VDC interface. Optical isolation is typically used to level shift between the voltage domains and provide galvanic isolation with a measure of protection against static electricity.

Repair Implications

Modular construction is an advantage for those who repair the PLC. Worn relays and damaged I/O semiconductors can be replaced. Damage such as inadvertently applying 120 VAC to a 24 VDC bus may be contained as opposed to spreading destruction into the logic board.

Don’t read too much into this statement. Crossing 120 VAC into the 24 VDC supply terminals will result is catastrophic damage that could ripple through the entire PLC.

Figure 3: Image of the Texas Instruments Tiva C microcontroller on the logic PCB.

:books: Continue Exploring Industrial Control Systems

If this discussion was helpful, you may also want to explore:

:world_map: DigiKey Navigation

:japanese_symbol_for_beginner: Related Foundational Articles

About This Author

Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.

Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.

Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.