A practical reference for technicians and engineers building, wiring, programming, and troubleshooting industrial control systems. This index is the navigation hub for industrial automation articles drawn from the DigiKey workbench and field experience. Content is organized by what you are trying to do — not by product category.
Use the difficulty icons to find your level:
Student →
Technician →
Engineer →
System Integrator
Last Update: 09 Nov 2026
Attention Educators: Structured learning pathways are available for selected field-guide content. While the field guide is organized by technical action and uses difficulty icons, the learning pathways arrange selected materials into learner-centric instructional sequences. Not all field-guide content is included in the pathways.
Core Hardware Platform for Training Labs
Related Training Kits
Construct a Three-Phase Motor Simulator
Starter Kit for the Siemens S7-1200 G2 Safety PLC: Parts & Build Guide
Latest Additions to the Field Guide
Why Does This PROFINET Cable Have Only Four Wires? A Siemens S7-1200 G2 Example
Identifying Different Metals Using an IO-Link Inductive Proximity Sensor
How to Find Compatible RJ45 Connectors for LAPP Ethernet Cables
Removing Industrial Ethernet Cable Jackets with a Sheathing Stripper
Industrial Ethernet Cable: Fixed Installation vs. Continuous Flex
How to Install a Shielded RJ45 Connector on Industrial CAT 6 Cable
Understand It
The physics, theory, and operating principles behind industrial control systems. No product agenda — just how things work and why. If you want to know what’s happening inside the contactor or why the AS-i bus faulted, start here.
Circuit Protection
Sensors
Reading Multiple Barcodes from the SICK SEC200 over TCP/IP
Introduction to the Inductive Proximity Sensor
Identifying Different Metals Using an IO-Link Inductive Proximity Sensor
Radar Tank Level Measurement: Lessons from a 55-Gallon Drum Experiment
Getting Started with Non-Contact Industrial Thermal Sensors
Sourcing and Sinking Configurations in Industrial Control Circuits
Applications of Type PNP and NPN Sensors
Connecting a 2-Wire Proximity Sensor to a PLC: What Can Go Wrong
Guide to Precision Encoders: From Quadrature to Hall
Quadrature Encoder
Relay Logic
Fundamentals
Teaching Electrical Nodes: Using 3D-Printed Wire Markers to Connect Wiring and Ladder Diagrams
Recommended Wire Colors for +24 VDC Industrial Control Labs
Exploring Polarity with DC Industrial Control Relays: A DigiKey Lab
Relay Normally Open vs Normally Closed Contacts
AC vs DC Relay Specifications: Coil Ratings, Contact Ratings, and Common Mistakes
Polarity and Flyback Protection in a 24 VDC Industrial Control Relay
Parallel Circuits in Industrial Controls: A DigiKey Lab
Teaching Node Voltage and Polarity with a Manual H-Bridge
Relay Jumpers Cut Wiring Time and Panel Clutter
Logic & Control
Timing & Sequencing
Circuit Theory
Motor & Contactor Behavior
PLC Scan Cycle & Memory
Safety Concepts
What are the attributes of an emergency stop pushbutton?
What Are Safety Door Interlocks? Wiring Standards and Tamper Protection Explained
How Are Light Curtains Mounted to Industrial Equipment?
How Are Light Curtains Aligned?
Finger vs Hand Light Curtains: Beam Spacing, Safety Distance, and Selection
Introduction to the Industrial Safety Relay
Getting Started with the Siemens Safety PLC
Network Fundamentals
24 VDC Control Power
Applied Theory
A Comprehensive Guide to Magnetic Field Behavior in Relays
Operation of the Latching Solenoid
H-Bridge Motor Drive Dynamics: Identification of Current Spikes
Visualizing Core Saturation and the Voltage-to-Frequency (V/f) Ratio
Guide to Ratiometric Sensor Applications
Permanent Magnets as an Energy-Saving Feature of a 3-Phase Motor Starter
Modeling PLC Digital Inputs: Transitioning from the Microcontroller to the PLC World
Wetting Current: Designing Reliable Industrial Inputs
Active-Clamp Flyback: Cutting Contactor Release Time by 79%
Potentiometer Linearization Series
EMI & Power Quality
Teardowns
Industrializing Microcontroller-Based Designs
Building Blocks of the 4-20 mA Industrial Ecosystem: SPI to Current Loop
Building Blocks of the 4-20 mA Industrial Ecosystem: Analog Transmitter
When to Use PCB-Mounted Relay Sockets
DIY PLC Components: Key Attributes of a 24 VDC Output Driver for Industrial Automation
The MOSFET Active Clamp: The Case Against a Relay’s Parallel Flyback Diode
Teach It
Structured learning for instructors and students with hardware in hand. Labs, guided Q&A sequences, and curriculum-aligned content. Not theory for its own sake — pedagogy with a workbench.
Kits
Industrial Automation Training Kit: Components and a Reusable Industrial Breadboard
Turn the DigiKey Industrial Automation Kit Into a Crouzet PLC Trainer
Construct a Three-Phase Motor Simulator
Starter Kit for the Siemens S7-1200 G2 Safety PLC: Parts & Build Guide
Getting Started with DigiKey’s Arduino Opta Kit
Shop Practices
A Reliable Ammeter Connection for 24 VDC Control Circuits
Stripping PUR Cable Without Nicking the Conductor Insulation
How to Install a Shielded RJ45 Connector on Industrial CAT 6 Cable
Industrial Ethernet Cable: Fixed Installation vs. Continuous Flex
How to Find Compatible RJ45 Connectors for LAPP Ethernet Cables
Why Does This PROFINET Cable Have Only Four Wires? A Siemens S7-1200 G2 Example
Removing Industrial Ethernet Cable Jackets with a Sheathing Stripper
Industry Context
Lab & Trainer Builds
Component Selection for Education
PLC Language for the Classroom
Showcase It
DigiKey demonstrator projects
- DigiKey Industrial Automation Demo: Interactive Sensors
- DigiKey Industrial Automation Demo: IO-Link Ball Float
- DigiKey Industrial Automation Demo: Siemens 3SK1 Safety Relay Demo
Select It
Choosing the right component for the job. Comparisons, selection guides, and specification walkthroughs. The product is the hero here — specific enough to act on.
PLCs
Are 12 VDC Programmable Logic Controllers (PLC) Available?
Software Compatibility Between the Arduino Opta and the Schneider Electric Modicon M171/M172 PLCs
How to Choose the Correct PLC
Beyond Specs: Soft Requirements for Selecting the Right PLC
Schneider Modicon M221 Programmable Logic Controller
Navigating Siemens S7-1200 PLC Model Numbers
Pilot Devices
Relays
Spring Terminal vs Screw Terminal Connections for Industrial Control Panels
What is a DIN Rail Relay?
What Is an Ice Cube Control Relay?
What Is an Octal Socket?
Beginner’s Guide to Selecting an Industrial Control Relay
An Engineer’s Perspective on Power Relays
Anatomy of a DC Solid-State Relay: Internal Design, Heat Limits, and Wiring Implications
Motor Drives (VFDs)
Panel Hardware
Networks & Comms
Power Supplies
Other
How to Choose a Fluke Multimeter or Process Calibrator for 4–20 mA Work
Different Size Pin Diameters in M8 and M12 Circular Connectors
Locating Siemens SMF Starters and MMS Switches for Fractional HP Motor Control
An Engineer’s Perspective on Power Transformers
Wireless Pushbuttons for Industrial Control Panels
Introduction to the Lighted Pushbutton for Industrial Control Panels
Start It
Platform-specific onramps for when the hardware just arrived. Unbox to first operation. Assumes you chose it already — this is how you get it running.
Integrate It
The convergence of electrical, network, and safety engineering. This category moves beyond physical installation to address systemic automation challenges: distributed I/O, network topology, and safety-rated signaling. We ensure every node is logically mapped, functionally validated, and architecturally secure.
Safety
Panel Construction
Terminal Blocks & Ferrules
I/O Wiring (sourcing/sinking)
Network Cabling (M8/M12)
Program It
Writing, structuring, and organizing control logic. Language-agnostic where possible — the concept is the hero, the platform is the support unless otherwise noted.
PLC
PLC Ladder Logic FAQs: A Practical Path from Beginner to Mastery
PLC Latches and the False Dichotomy Between Set/Reset and Traditional Logic
Guide to Programming a PLC in C++: Cycle Scan
PLC Programming Language Introduction
PLC Control Terminology: Define Signals by Time and Logic
Siemens S7-1200 and S7-1500
Make Your PLC Play a Song: Mastering Siemens PLC Memory Arrays
Building a State Machine in Function Block Diagram Using Siemens TIA Portal
Using Ladder Logic Rung with Multiple Serial Connected Coils
How to Configure the FirstScan Bit in Siemens TIA Portal
Understanding the Siemens Data Block (DB) File Format in TIA Portal
Siemens LOGO!
Schneider Zelio
Schneider Modicon
Introduction to the Modicon PLC UDFB
Introduction to the Schneider Electric TMH2GDB HMI for the Modicon M221 Nano PLC
Integrating the Banner K50 Pro Optical Series Touch Button with a Schneider Modicon PLC
How to Configure the Modicon PLC for a Quadrature Encoder
Single Pushbutton On-Off Control Including a Ladder Logic Demo in the Modicon PLC
Crouzet
Why won’t Crouzet-Soft connect to the networked Crouzet PLC?
Cell Phone Control of a Crouzet PLC Using Bluetooth
Prevent Unexpected Equipment Start-Up with Defensive PLC Programming
Power-On Safety Macro for the Crouzet PLC
Crouzet Sequential Function Chart Macro for a Three-Phase Motor Starter
Introduction to Crouzet PLC Sequential Function Chart (SFC) Programming
PLC Finite State Machine Control Using a Sequence Cam Block
Arduino Opta
Refer to the manufacturer’s information to get started:
- PLC IDE: Getting started with Finder OPTA and PLC IDE - Finder OPTA
- Arduino IDE: Getting Started with Opta™ - Finder OPTA
DigiKey Resources:
Beginner’s Guide to Connecting Outputs with Arduino Opta PLC
Beginner’s Guide to Connecting Digital Inputs to the Arduino Opta PLC
Mapping DigiKey’s Opta PLC Trainer to the Arduino Academy ACE-100 Course
Arduino Opta PLC Ladder Logic Memory Structures
Ladder Logic UDFB in the Arduino Opta PLC
How to View I/O Status on the Arduino Opta
Programming a PLC in C++: Pointer Injection for Structured Handling of Digital I/O
State Machines
Data Structures (UDT/DB)
PID & Analog
Networks & Protocols
You Don’t [Always] Need to Import the IODD File for IO-Link
Distributed Intelligence in an IO-Link System
Understanding the IO-Link I/O Device Description (IODD) File
What Software Files Are Required for IO-Link?
Runtime Network Health Monitoring Between a Siemens S7 and LOGO! PLC
Scalable Modbus Architecture in TIA Portal: The Nth Device Strategy
Distributed I/O
Peripherals & Smart Devices
Measure It
Multimeter Fuse Replacement: Use the OEM-Recommended Fuse, No Substitutions
Introduction to Megger Insulation Resistance Tester for Motor and Cable Testing
Understanding Thermal Imaging for Electrical Inspections
Process Meter First Steps: Source vs. Simulate Mode in a 4-20 mA Loop
Troubleshoot It
Something is wrong and you need to find it. Fault patterns, diagnostic techniques, and real failure modes from the bench. Assumes you know how it should work.
Relays & Contactors
Power Supplies
Safety Systems
Certify It
Compliance, standards, and documentation for panels and systems that need to meet a code. UL, SCCR, and inspection-readiness.
Human Factors
UL 508A
Peak Let-Through Current FAQs for UL 508A Industrial Control Panel Fuses
Integrating a 120 VAC Programming Receptacle into a UL 508A Listed Control Panel
Circuit Breaker Branch Protection vs. Supplementary Protector in a UL 508A Listed Control Panel
Navigating UL 508A for Industrial Control Panel Enclosures