Please identify this connector for me

I need this connector for an audison amplifier. I found some products on the digikey website but can’t be sure. I’m hoping that to some of you, it would be like second nature to identify this connector.

I have attached one photo of the actual connector and one photo from the manual of the amplifier.

Fingers crossed and thank you!


Hello @Mastamoe

Welcome to the TechForum

I have found 2 parts that have the same keying as the connector for your amplifier they are part number 1716920102 and part number 0430250210. The one thing you will have to check is the pitch of the connector you have as these parts have different pitches. the pitch is the distance from the center of the pin to the center of the other pin.

Thank you very much for your response. I was able to measure the pitch of the connector on the amplifier. Its 3mm, so I need 0430250210.

Do you offer this connector with leads? Not sure if you would refer to that as a pigtail or not.

Would it be 2147551023?

Yes, the 2147551023 would be an option. It has an identical Micro-Fit 3.0 Female connector on each end and a set of 600mm (23.6") black 18 AWG wires attached in-between.

If you had a different preference for length, or prefer gold contacts, here are some otherwise identical options.

Image of 2147551023

If you would rather insert the crimped jumper wires yourself, we have additional options here for those, which include options for length, color, wire gauge (20 AWG ~ 24 AWG), and having crimps on one or both ends.

Image of pre-crimped Micro-Fit 3.0 jumper wire with crimp on each end