Finding connector

I need help finding the right connector. I’m looking for a connector that has two versions: one for wire-to-wire connection and one for box mount. It needs to have between 33 and 40 pins, similar to those used in automotive applications. I was considering the TE Connectivity AMP Connectors, product numbers 1743059-2 and 1743060-2, but unfortunately, they don’t have the box mount type.

Hello dupontmaxime47,

Welcome to the DigiKey TechForum.
The closest I found for a panel mount connector is 889-ATV04-38PA-S2-ND, and the mating connector is 889-ATV06-38SA-S2-ND. I did not find a free hanging version of the first part number, but you don’t have to mount it in a panel to work.
Please check the datasheets.

Yes, I understand that it would work if it weren’t on a panel, but that’s not what I wanted. Thanks for your help anyway.

Hello! I am searching for a Panasonic Home Theater speaker connector. Closest thing i found on the internet are the Reex1266a, but they are super expensive. Can you help me find an alternative please?

Hello,
Welcome to the DigiKey TechForum . Can you provide us with a photo of the connector you have and any markings that may be on it ?

image

it looks something like this, there is no marking on it. i know its a 4.2mm pitch. And its approximatly the size of a usb plug.

Hello @mathieu.therrien

I did not find a connector on our site like Reex1266a.

a little Molex 4.2mm pitch with crimp should do it?

The connectors for home theater sound systems tend to be available from after market vendors like Ebay and Amazon. To find the correct connector try searching “your model number” + speaker connector.

These home theater speaker connectors are not something that we carry.

yeah i understand that, i found them on Ebay but they are too expensive, that it why i want to buy some Molex and try to make them fit in there. Its an old Home Theater and i don’t care if i bend the pins a little bit. Can you recommend me a small size molex plug with tin crimp, 4.2mm pitch please?

You can take your pick of the different selection of these connectors from Molex.

Thank you! I found one that fit perfectly, can you help me find a tin crimp who fits in this Molex please?

DigiKey Part Number
900-0469920220-ND

16awg wire 16awg wire

Hello Again
These are the options for have available for 16awg

These are the associated 16 AWG contacts for this connector.

thank you so much, very good service, very helpful. big big big thank you!