I working on a system for WIFI. The system uses POE injection. Receiver is 24v with max of 7 watts 0.3 amps max and Transmitter is 48v 9 watts 0.5 amps max. If Im reading correctly it seems as though the Tycon RPPL1224-36-35 offers POE power of 24v or 48 v. Is there a way that I could supply both without the addition of the added power consumption of an inverter and POE injectors? this is my first build with solar to power these units so I need advice please.