Hi All - I’m in urgent need of some help to identify pull to seat barrel terminals from a 2022 Honda Civic Touring. These were taken from a Molex adapter using the standard removal tool. The diameter of the wire looks to be 20-22 gauge, and I don’t see any markings on the molex adapter nor the terminals.
Are you able to provide a picture and dimensions of the housing for the contacts? It will be helpful in finding the contacts.
Hello Rhonda - I have a digital caliper I can take measurements with. Do you prefer the terminal measurements or the molex connector?
Hello,
We would need the pitch of the connector. This would be measured from the center of one pin to the center of the next one. We can only pick out terminals if we know what the housing is. My guess this could be a proprietary connector. We can try with the additional information. We would need information on the housing only.
It appears to be 4mm from center-to-center of the terminal openings.
Unfortunately I do not find this one in our system. Though others do monitor the forum. Maybe someone else might have an idea how to identify this part.
Hi Verna -
These terminals look to be exactly what I need, but they aren’t available.
The are listed as 3-Pin Connector Kit for Honda K-Series K20 Crank Position Sensor Plug Clip
https://www.amazon.com/3-Pin-Connector-Honda-Position-Sensor/dp/B07S42158G
I found them, along with many other specialty connectors, at https://www.ksvlooms.com/