We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
Radiant heat system in soffit of home about 7’ off floor. Not efficient - heat rising to ceiling peak. Goal: small - less than 6" - fan that can either be hard wired, or battery powered (better), that can be controlled by a remote switch to turn on and off.
As a room warms up, remote could switch on the fan for cycles of time until desired room temperature is reached. I don’t think high revolutions are needed… I would want to keep fan noise at a minimum too.
An internet search for “remote control outlet” should return results for a fair number of finished-goods consumer products that allow control of an AC circuit using a remote control device, and small AC fans are likely also available at many of the retailers that would carry such products. Such an approach would likely give you a reasonable result for less cost and effort than assembling a solution from component-level products of the sort which are Digi-Key’s primary product of trade. Standard ceiling fans with remote control features are also available, and might be a good option if space permits.
Small-diameter fans don’t move a great deal of air, and tend to make a relatively large amount of noise in the process of doing so. They also consume a fair bit of electricity, so a battery-powered unit likely to give a decent result in terms of comfort level would probably require frequent battery changes, and prove unsatisfying from that perspective.
This said, if you would still like to pursue a more build-it-yourself sort of solution, FOBLOQF-4S1-ND is a single-channel remote control device which might be suitable. Similar devices offering multiple control channels are also available.