Raspberry Pi 400 with Chromium OS and Optional Accessories

The Pi 400 is a Raspberry Pi built into a 78 or 79-key Keyboard depending on the region with the following features

The processor is the Broadcom BCM2711, Quad-Core 64-bit SoC (Arm Cortex-A72 @ 1.8GHz)
The memory RAM included is 4GB LPDDR4-3200
The connectivity options are wireless LAN (Dual-Band 2.4Ghz and 5.0Ghz) IEEE 802.11 B/G/N/AC Bluetooth 5.1, BLE
Gigabit Ethernet

1 x 40 pin GPIO Header

1 x MicroSD Card Slot

2 x Micro HDMI Connections

1 x USB-C Connector for 5V Power

2 x USB 3.0

1 x USB 2.0

1 x Ethernet connector

image

 

Capture
Datasheet

 

 
Capture
 
 
2648-SC0272-ND
 

Other HDMI-A Male to Micro HDMI-D Male Cable options can be found here,

 

 


1690-RPIUSB-CPOWERSUPPLYBLACKUS-ND

 

Other USB-C adapter options AC DC Desktop, Wall Power Adapters | Electronic Components Distributor DigiKey

 

You can use a wired mouse such as

image
1690-RPI-MOUSERED-ND

Wireless Mouse options here Computer Mouse, Trackballs | Electronic Components Distributor DigiKey
 

 

I tested the Pi 400 out with the Chromium OS found here Releases · FydeOS/chromium_os-raspberry_pi · GitHub with the image file name chromiumos_image_r86r2-rpi4b.img.xz . If you plan on testing this OS with the Pi, just download the img file and upload with the Raspberry Pi Imager found here Introducing Raspberry Pi Imager, our new imaging utility - Raspberry Pi. In the Raspberry Pi Imager select “Use Custom” under Operating System then find the Chromium OS image in the downloads folder then write that file to the microsd card as seen below.


 

 


 

 


 

 

 

 

Applicable part numbers
SC0372,
SC0373, SC0376, SC0374, SC0375, SC0377
 

 

 
Related post
Raspberry Pi boards - FAQs - Engineering and Component Solution Forum - TechForum │ Digi-Key

Differences in Raspberry Pi Compute Boards - FAQs - Engineering and Component Solution Forum - TechForum │ Digi-Key

Nice post, Jeffery!