We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I am trying to identify source for a magnetic field sensor which operates off 5V and has a ratiomatic signal output between 500mV and 4500mV depending on the proximity of a magnet.
The component has what looks like chips connected together with six open conductors and also the three conductors for the +5v VCC, ground, and signal connections.
The markings are as appears on the top section to be 17505 with what appears to be KMA 21C m2991 T01 on the bottom section.
It’s almost certainly an NXP sensor. These two look similar (KMA210:115, KMA215,118) though I can’t yet tell if it might be one of them or another related part. Assuming that the “C” might be a zero, it may well be the KMA210, but it looks like there are several variants. Also, unfortunately they are all obsolete.