I’m looking for replacement capacitors for a old motherboard of mine. I can’t find the esr rating for the caps in the data sheet.
Electrolytic I was looking at
United Chemi-Con
I was thinking of doing polymer. The one I found is only 2.5V and is only 2000 hours @ 105C life instead of the 5000. I know the basics and I think these caps are output filtering. I’d think that they wouldn’t be getting more than 2.5V as the vcore is 1.35V
The parameters for the existing caps:
through hole
kzg nichicon
6.3V
10mm Diameter
5mm lead spacing
3300uf