Référence produit équivalent gyroscope/accéléromètre

Bonjour,

Je suis à la recherche d’un produit peut être proposé par Digikey de préférence qui a exactement les même caractéristiques que ce produit ou peut être meilleur :

SparkFun VR IMU Breakout - BNO086 (Qwiic)

Voici le lien du produit de référence : SparkFun VR IMU Breakout - BNO086 (Qwiic)

Je cherche une alternative avec exactement les mêmes caratéristiques ou mieux, un Gyroscope accéléromètre, magnétomètre.

Merci, Cordialement

In english :

Hello,

I am looking for a product that can be offered by Digikey preferably that has exactly the same characteristics as this product or can be better:

SparkFun VR IMU Breakout - BNO086 (Qwiic)

Here is the link to the reference product : SparkFun VR IMU Breakout - BNO086 (Qwiic)

I am looking for an alternative with exactly the same characteristics or better, a Gyroscope accelerometer, magnetometer.

Best regards

Hello Laserfight,

The only other board I was able to find that has a Accelerometer, Gyroscope, Magnetometer and utilizes the BNO086 is 1888-BNO086DEVKIT-ND but because it is not SparkFun it will not utilize Qwiic Interconnect system. I did find a couple other options that have the Accelerometer, Gyroscope, Magnetometer function and use Qwiic platform but they do not utilize the BNO086, these options can be found HERE. Hopefully this helps but let us know if you have any further questions.

While the Sparkfun VR IMU uses the BNO086, it is a drop in replacement for the BNO085. The features that the BNO086 offers over the BNO085 are 14-bit accelerometer fusion, reduced idle state power and Interactive Calibration.

The BNO085 could be used in the interim while waiting for the BNO086 IMU to become available.

Adafruit has 1528-4754-ND as an available option.

Hi thank you and,
This option is good ? : BNO055 Bosch Sensortec | Capteurs, transducteurs | DigiKey

Hello laserfight

BNO055 is another option.
There is a breakout board from Adafruit Industries LLC, 1528-1426-ND.
Please verify with the datasheets.