I am going to be installing a radon mitigation system, with the fan in the attic, which is largely inaccessible. The electrical feed for the fan will originate at the main electrical panel in the basement. We want to monitor the fan to ensure that it is operating via the home security/alarm system.
I am a retired electrician. I thought I could put a small current transformer in the circuit breaker panel that would feed a relay with a contact which would open on loss of power.
The fan is designed to run continuously, should the fan motor fail, it should go into a locked rotor state tripping the breaker.
I would not want to create a spurious alarm with loss of normal utility power, until our whole home emergency generator picked up the load – so a relay with a time delay?
Would you be able to recommend some components which I could accomplish this with?
All thoughts are sincerely appreciated,