I have a Champion 2800/4000 portable generator with dual 20 Amp breakers, one of which has a broken lever and needs to be replaced. The original breaker is an:
AIRPAX LEG6-1-61F-20.0-A-01-V
I used a post on this forum to parse this part number to be:
- On toggle handle per unit
- Single pole
- Series
- 50/60 Hz Short Delay
- Inertial delay
- 20.0 Amp Rated Current
- Metric thread terminals
- Black on/off Marked
- VDE and CCC Approved
Other markings include:
- Max, V 125 50/60
- Trip Curve 61F
- Trip Amps 25
- AIC 5000 A/C
- Special Purpose, Not for General Use, Vert. Mount Only
I don’t know if this exact same breaker is still available but I could not find it and so I suspect it is not current. However, I am sure there is a reasonable replacement and I would like help identifying it. I see lots of similar-looking options on Digi-Key’s parts list but I can’t be sure of what to order. I suppose the replacement could be another brand, but then I wouldn’t know how to start figuring that out.
In consideration of a replacement, if possible, I would like to get a breaker that resists breaking as quickly. This current breaker often trips off with certain equipment even though the engine is not working hard. I’m not sure what is needed but maybe a longer “delay” or maybe higher tripping Amps.
I will appreciate any assistance that can be provided.
Brian v.