I am trying to find the following or something that is compatible:
(1.) SANKEN-AIRPAX UPG 1, I n 30A, U e 250 V, Hz 50/60, D 600, T/A 37.5 A: Replacement Breaker IUG1-1-63-30.0-A-01
(2.) SANKEN-AIRPAX UPG 1, I n 20A, U e 250 V, Hz 50/60, D 600, T/A 25.0 A: Replacement Breaker IUG1-1-63-20.0-A-01
We have a possible alternate for the 30A, with the quick connect terminals, which is 723-1159-ND. This one has a white toggle lever.
The possible alternate for the 20A, has screw terminals, which is 723-1291-ND. This one has a black lever.
If you want a 30A with a black lever to match, it will have screw terminals, which is 723-1546-ND.
Please check the datasheets.
Thank you for the information. Can you confirm that the possible alternate for the 20A, has screw terminals, which is 723-1291-N matches my existing breaker (see attached photo)?
Best regards,
Angela
Live life, don’t just exist.
HI will-live_ez ,
Based on the photo, they look like they would match, please review datasheet.