Replacement capacitors needed for video card

I have a Zotac GTX1060 video card which I believe has blown capacitors. There was a puff of smoke then a very strong foul smell.

There are 6 caps that are red and grey with the fallowing numbers.
818Z
1200
25

There are 4 caps that are red and grey with the fallowing numbers.
725Z
330
16

There is 1 cap that is red and grey with the fallowing numbers.
560
6.3v
RL808

I have tried Google searching the numbers and got nothing pertaining to capacitors. Could someone please help me find suitable replacements?

Are you able to send pictures of the caps?
Also, physical size will help. Diameter, height, lead spacing.

1 Like

UKL1C331KPDANA is 330uF 16V
UPA1V122MHD1TO is 35V 1200UF
UPJ1C561MPD is 16V 560UF
See if these look like what you need. I went up in voltage where I could.

1 Like

Thanks for the quick response Rhonda. Here are the pics you requested just to make sure. I know how to solder but I do not know anything about this stuff at all unfortunately. I was told the hardest part is finding the right caps. Which after looking at things I can see they are really easy to solder in.