Replacement of IGBT components on my treadmill

Hello I would like to replace a defective component on the motor control board MC2100ELS-18W of my treadmill nordicktrac s20i. I could not find the component in your website. The component I need to replace is an IGBT from NCE (600V, 60A, Trench FS II Fast IGBT, TO 247, ref= NCE60TD60BT). Can you help me to find a similar component or if not the same a more powerful one.
2004201607_Wuxi-NCE-Power-Semiconductor-NCE60TD60BT_C502946.pdf (666.0 KB)
Thank you for your support
2004201607_Wuxi-NCE-Power-Semiconductor-NCE60TD60BT_C502946.pdf (666.0 KB)

Hello,

I could not come up with replacements for these.

Thank you for checking.
Is there an alternative if the same does not exist?

Hi zakaria_belbakra,

No guarantees, but the IGW75N65H5XKSA1 seems to be a fairly similar part. A couple others which are also worth a look are these:

FGH75T65SHDT-F155
IXYH50N65C3H1

Make note that just replacing the IGBTs isn’t guaranteed to fix your board, as other things may have also been damaged.

Thank you very much David for the references.
I will order one of them and see what happened. I will let you know.

It’s not a problem if I put a 650V instead of a 600V?

An IGBT rated for 650V max, can be used in place of a 600V rated IGBT.

Correct. Higher voltage rating just allows for 50V of extra safety margin. That value represents the highest voltage the device can handle without causing damage,

Super, it’s what I need. I hope it will work.

@zakaria_belbakra

Let us know how it goes!

Hello,
Coming back from my treadmill issue. Unfortunately the replacement of the part solved partially my issue. The treadmill is not anymore crashing when I start it as before but when it doesn’t want to run. When i push on start, it’s doing nothing. I think I will by a new board since it will take time and cost more money if I continue to try to troubleshoot it. Thank you for your help.
Best regards
Zak

Thank you for coming back and letting us know how it turned out.