Reset button replacement | Aruba 2930F Switch

I’m looking for a replacement for the button highlighted on the right. There is a similar one on the left, and that still works (for reference). It seems like these are surface mounted. I can take more pictures if needed. These are from an Aruba 2930F switch, and they are used to reset the device.
Any help is greatly appreciated.

Welcome to the community!

Do you know what the outline dimensions are? We have several tactile switches that look similar, but we would need to know the dimensions. One can take a look at the similar options here and use the “outline” filter to narrow the results.
image


Would it be fair to say that it measures something between 3~4 mm where it has the button and around 3 mm on the other side?

The following switch looks similar, see if it will work for you.

PTS841 GK SMTR LFS C&K | Switches | DigiKey