Resistor Kit values E24/E96

------Question for RC0402FR-SNE96L Please Put your question below------

Where can i get the list of values/numbers in the kit?

Hello @c.ludwig
Welcome to DigiKey’s TechForum,

The resistance range can be noted on the product page - 0 ~ 10M
The quantity is defined as 100 pieces per value with 300 values per kit.

Regarding specific values for the E series the EIA Standard will denote the base value. This base value multiplied or divided by powers of ten referred to as decade scaling.
Base Values: See Chart Here These values apply across all magnitudes—0.1Ω, 1Ω, 10Ω, 100Ω, 1kΩ, 10kΩ, etc..

Datasheet Link

Related TechForum post - What is the difference in “E” series values for resistors?

The E96 has 96 Values per decade. The range of the kit RC0402FR‐SNE96L has 7 decades (1R to 10M) resulting in 672 values. The E24 series has 168 values in the 1R..10M -range.
The Kit RC0402FR‐SNE96L has 300 resistor values regarding to the datasheet -somwhere between E96 and E24.
The simple question is: Which values of th E96 series are available in the RC0402FR‐SNE96L.
There must be an table of contents…