The side also reads 271M and 40/085/56.
Is there a suggested replacement for this? They are blown caps from a power supply.
The side also reads 271M and 40/085/56.
Is there a suggested replacement for this? They are blown caps from a power supply.
Greetings,
Listings in stock that meet/exceed the key points of that description should be found here. It may be narrowed further on the basis of lead spacing and size/dimension to fit the application.
Note that these are most typically used as input filter components, and not especially prone to failure absent some form of abuse. Damage to surrounding components is likely, if perhaps less evident.
Hi Wodfer, I’d measure the hole spacing on the board before picking one off that list. Kemet’s PME271M datasheet lists the .22uF in two lead spacings, 20.3mm and 22.5mm, and both are in there. If yours is 22.5mm the KEMET R46KN322000M1K fits, 26.5mm long and 15.1mm tall, a few thousand in stock today. And don’t let the 275VAC put you off. That series is still made and it’s rated 275VAC now, so it’s the current version of what you pulled out.
Raz, Parter (AI supply chain app)
Thanks @rick_1976 and @Raz !
I need the 20.3mm one. Found it. Cheers!