Capacitors

I need help identifying these capacitors, which are from an air filtration system. If someone could give me links to the actual capacitors on DigiKey, it would be greatly appreciated. lead spacing 1.1", size 3/4"x1.25"x3/8"

s

Hello @larrypac1,

For the MPE 225k 250v -40 to 105c, please review alternative options here.

For the .1K 275V X2 safety cap, please review the alterantive options here.
MPX104K305D might be a suitable option. Please review the datasheet before ordering.

Thanks!

Regarding 225K 250V option you may be interested in F863FL225K310Z having longer leads may be suitable for laying on its side like your photo.

Thanks for taking the time to help with such a small order. The lead spacing was a bit off on one of the ones you linked, but I found the two capacitors below which seem to be a better match for the numbers, but I know next to nothing about capacitance or how important voltage is. Would you mind taking a look? I’m pasting the original specs below the product numbers. This is for an air filtration system.

PHE820EB6100KR17# R46KR422050P0MI need help identifying these capacitors, which are from an air filtration system. If someone could give me links to the actual capacitors on Digikey, it would be greatly appreciated. Orange one specs: lead spacing 1.1", size 3/4"x1.25"x3/8"

yellow one specs: 3/4"x1/2"x 1/4", lead spacing 15mm (5/8")

Please disregard my email sent a few minutes ago. I went ahead and ordered 2 capacitors and hopefully they will work. If not, it won’t break the bank. Thanks for taking the time. larry