Description
This project sets up a Seeed Wio Terminal as a remote outdoor air quality display that shows ozone (O3) and Particulate Matter (PM2.5 and PM10) data. The Wio Terminal receives AQI data over WiFi by subscribing to live sensor data using MQTT with Machinechat’s JEDI One IoT data platform. Arduino is used to implement the Wio Terminal application and JEDI One is installed and running on a Raspberry Pi 4.
Hardware
- RASPBERRY PI 4B/4GB
Raspberry PI 4 Model B with 4GB SDRAM - Seeed Wio Terminal
Wio Terminal is a standalone Arduino/MicroPython compatible SAMD51-based microcontroller evaluation platform with WiFi/Bluetooth powered by a Realtek RTL8720DN. It is equipped with a 2.4” LCD Screen, onboard IMU(LIS3DHTR), Microphone, Buzzer, microSD card slot, Light sensor, and Infrared Emitter(IR 940nm).
Software
- JEDI One
JEDI One is a ready-to-use IoT data management software solution. Capabilities include: collect data from sensors, devices and machines; build intuitive real-time and historical data and system view dashboards; create rules to monitor and respond to data conditions automatically; receive alert notifications by email and SMS. - Arduino
Arduino is an open-source electronics platform based on easy-to-use hardware and software.
Background
The primary air pollutants monitored by the US Environmental Protection Agency(EPA) monitors are ozone and Particulate Matter. Below map from https://www.airnow.gov/ is an interactive GUI that provides information on air quality throughout the US.
Ground-level ozone can trigger a variety of health problems, particularly for children, the elderly, and people of all ages who have lung diseases such as asthma. Particulate matter (PM2.5 and PM10) contains microscopic solids or liquid droplets that can be inhaled and cause serious health problems.
Implementation
The project uses a Wio Terminal to implement a remote outdoor air quality display and Arduino is used to implement the code. The Wio Terminal is set up to connect over WiFi to the MQTT broker running on the JEDI One. Once connected, it subscribes to ozone and PM air quality sensor data being collected by the JEDI One. The LCD display is used to provide air quality information as shown below.
The display shows AQI values, color coded AQI level, color coded timestamp of the most recent data received and a rolling two value chart showing the last 50 sensor readings. The JEDI One is also configured to display the sensor data in widgets on the Sensor Dashboard.
Note: This project builds on two other Machinechat sensor projects that provide ozone and PM data to Machinechat’s JEDI One IoT Data Platform. First project is Machinechat with Renesas ZMOD4510 Outdoor Air Quality Sensor. Second project is Machinechat with Panasonic SN-GCJA5 Air Quality (PM) Sensor.
Set up the Wio Terminal platform for the Arduino application
1 - Set up Arduino on the Wio Terminal. See link Getting started with Wio Terminal
note: make sure Realtek RTL8720DN firmware is updated per Update the Wireless Core Firmware
2 - Install libraries needed for application. Add these libraries thru Arduino’s Library Manager:
- Adafruit Zero DMA
- Seeed_Arduino_Linechart
- ArduinoJson
- PubSubClient
Libraries needed for WiFi - Seeed_Arduino_rpcWiFi
- Seeed_Arduino_rpcUnified
- Seeed_Arduino_mbedtls
- Seeed_Arduino_FS
- Seeed_Arduino_SFUD
note: add “Free_Fonts.h” and “arduino_secrets.h” files to project directory (Free_Fonts.h is located in ~/Arduino/libraries/Seeed_LCD_master/examples/320 x 240/All_Free_Fonts_Demo)
3 - Code walkthrough (filename: WioTerminalMQTTDisplay2topicOAQrev2.ino)
Setup LCD display, connect to WiFi network, connect to MQTT broker and parse JSON MQTT messages
/*
Wio Terminal MQTT data display example
filename: WioTerminalMQTTDisplay2topicOAQ.ino
project based on WioTerminalMQTTDisplay.ino which is a sketch that demonstrates using the Wio Terminal to mqtt subscribe to air quality sensor data on the
machinechat JEDI One IoT data platform. It uses WiFi to connect to the JEDI One MQTT broker.
Ozone air quality sensor data - Renesas
Particle air quality sensor date - Panasonic
11/10/2021 - this project takes sketch WioTerminalMQTTDisplay.ino and modifies to subscribe to 2 topics and changes topics to outdoor air quality sensors for
ozone and particulate matter to display AQI
11/16/2021 - clean up code and change to version to "_rev1", also add 3rd subtopic for testing
3/30/2022 - rev2 change back to subscribe to just two topics (comment out subtopic1
*/
#include <rpcWiFi.h>
#include <PubSubClient.h>
#include <TFT_eSPI.h>
#include "Free_Fonts.h"
#include"seeed_line_chart.h" //include the library
TFT_eSPI tft;
// for LCD line chart
#define max_size 50 //maximum size of data
doubles data[2]; //Initilising a doubles type to store data
TFT_eSprite spr = TFT_eSprite(&tft); // Sprite
char value[7] = " "; //initial values
char value2[7] = " ";
char stamp[40] = "2021-09-01T13:04:34";
//#include <ESP8266WiFi.h>
//#include <PubSubClient.h>
#include <ArduinoJson.h>
#include "arduino_secrets.h"
// Update these with values suitable for your network.
char ssid[] = SECRET_SSID; // your network SSID (name)
char pass[] = SECRET_PASS; // your network password (use for WPA, or use as key for WEP)
// MQTT server info for JEDI One
const char* mqttServer = "192.168.1.7";
const int mqttPort = 1883;
StaticJsonDocument<256> doc;
int data1 = 0; //data1 of MQTT json message
int data2 = 0; //data2 of MQTT json message
int data3 = 0; //data3 of MQTT json message
int data4 = 0; //data3 of MQTT json message
int msg = 0;
const char* timestamp = "dummy data"; //the is the MQTT message timestamp (this works)
String recv_payload;
const char* subtopic1 = "datacache/T960981B2D"; //pump house humidity, temp sensor
const char* subtopic2 = "datacache/MKR1010_Z4510oaq2S31PMOD"; //ZMOD4510 air quality/ozone sensor
const char* subtopic3 = "datacache/MKR1010WiFiSensor_SNGCJA5"; //SNGCJA5x air quality particl sensor
// wio terminal wifi
WiFiClient wclient;
PubSubClient client(wclient); // Setup MQTT client
void setup_wifi() {
delay(10);
// We start by connecting to a WiFi network
Serial.println();
Serial.print("Connecting to ");
Serial.println(ssid);
WiFi.mode(WIFI_STA);
WiFi.begin(ssid, pass);
while (WiFi.status() != WL_CONNECTED) {
delay(500);
Serial.print(".");
}
randomSeed(micros());
Serial.println("");
Serial.println("WiFi connected");
Serial.println("IP address: ");
Serial.println(WiFi.localIP());
}
// mqtt message callback
void callback(char* topic, byte* payload, unsigned int length) {
//print out message topic and payload
Serial.print("New message from Subscribe topic: ");
Serial.println(topic);
Serial.print("Subscribe JSON payload: ");
for (int i = 0; i < length; i++) {
Serial.print((char)payload[i]); // print mqtt payload
}
Serial.println();
msg = 1; //set message flag = 1 when new subscribe message received
//check subscribe topic for message received and decode
//********************************//
//if message from topic subtopic1
//********************************//
if (strcmp(topic, subtopic1)== 0) {
// "clear" old data by rewriting old info in white
tft.setTextColor(TFT_WHITE); //"clear" old data by rewriting old info in white
tft.setFreeFont(FF19);
tft.drawString(value,200,78);
//tft.drawString(value2,60,78); //value2 is same as data2
tft.setFreeFont(FF18);
tft.drawString(stamp,60,110);
Serial.print("decode payload from topic ");
Serial.println(topic);
deserializeJson(doc, (const byte*)payload, length); //parse MQTT message
data1 = doc["data1"]; // data1 is humidity
//data2 = data4; // data4 is O3 FastAQI
//data2 = doc["data2"]; // data2 is temp
//data3 = doc["data3"]; // data3 is empty
timestamp = doc["timestamp"]; //mqtt message timestamp
// stamp = timestamp;
strcpy (stamp,timestamp);
stamp[19] = 0; // terminate string after seconds
Serial.println(stamp); //debug print
tft.setTextColor(TFT_MAGENTA);
tft.setFreeFont(FF19);
itoa(data1,value,10); //convert data integer value to character
tft.drawString(value,200,78);//prints data at (x,y)
//itoa(data2,value2,10);
//tft.setTextColor(TFT_BLUE);
//tft.drawString(value2,60,78);
tft.setTextColor(TFT_BLACK);
tft.setFreeFont(FF18);
tft.drawString(stamp,60,110); //print timestamp
}
//********************************//
//if message from topic subtopic2
//********************************//
if (strcmp(topic, subtopic2)== 0) {
// "clear" old data by rewriting old info in white
tft.setTextColor(TFT_WHITE); //"clear" old data by rewriting old info in white
tft.setFreeFont(FF19);
tft.drawString(value2,50,78); //"clear" old value2 (is same as data2)
tft.setFreeFont(FF18);
tft.drawString(stamp,60,110); //"clear" old timestamp
Serial.print("decode payload from topic ");
Serial.println(topic);
deserializeJson(doc, (const byte*)payload, length); //parse MQTT message
// data1 = doc["data1"];
data2 = doc["FastAQI"]; //
itoa(data2,value2,10);
tft.setFreeFont(FF19);
tft.setTextColor(TFT_BLUE);
tft.drawString(value2,50,78); //print new value2 on LCD
Serial.print("data2 is O3 FastAQI = ");
Serial.println(data2);
timestamp = doc["timestamp"]; //mqtt message timestamp
// stamp = timestamp;
strcpy (stamp,timestamp);
stamp[19] = 0; // terminate string after seconds
tft.setTextColor(TFT_BLUE);
tft.setFreeFont(FF18);
tft.drawString(stamp,60,110); //print new timestamp on LCD
//print out color of "AQI" font based on value of AQI
// <50=green,51to100=yellow,101to150=orange,>150=red
if (data2 < 51) {
tft.setTextColor(TFT_GREEN);
}
else if (data2 < 101){
tft.setTextColor(TFT_YELLOW);
}
else if (data2 < 151){
tft.setTextColor(TFT_ORANGE);
}
else {
tft.setTextColor(TFT_RED);
}
tft.setFreeFont(FF18);
tft.drawString("AQI",100,78);
}
//********************************//
//if message from topic subtopic3
//********************************//
if (strcmp(topic, subtopic3)== 0) {
// "clear" old data by rewriting old info in white
tft.setTextColor(TFT_WHITE); //"clear" old data by rewriting old info in white
tft.setFreeFont(FF19);
tft.drawString(value,200,78); //"clear" old value
tft.setFreeFont(FF18);
tft.drawString(stamp,60,110); //"clear" old timestamp
Serial.print("decode payload from topic ");
Serial.println(topic);
deserializeJson(doc, (const byte*)payload, length); //parse MQTT message
data3 = doc["aqiPM2_5"];
data4 = doc["aqiPM10"];
Serial.print("data3 = aqiPM2_5 = ");
Serial.println(data3);
Serial.print("data4 = aqiPM10 = ");
Serial.println(data4);
// determine which PM2.5 or PM10 is larger to use when displaying PM AQI
if (data3 >= data4) {
data1 = data3;
}
else {
data1 = data4;
}
Serial.print("Particle AQI = ");
Serial.println(data1);
tft.setTextColor(TFT_MAGENTA);
tft.setFreeFont(FF19);
itoa(data1,value,10); //convert data integer to character "value"
tft.drawString(value,200,78);//prints "value" at (x,y)
timestamp = doc["timestamp"]; //mqtt message timestamp
strcpy (stamp,timestamp);
stamp[19] = 0; // terminate string after seconds
tft.setTextColor(TFT_MAGENTA);
tft.setFreeFont(FF18);
tft.drawString(stamp,60,110); //print new timestamp on LCD
//print out color of "AQI" font based on value of AQI
// <50=green,51to100=yellow,101to150=orange,>150=red
if (data1 < 51) {
tft.setTextColor(TFT_GREEN);
}
else if (data1 < 101){
tft.setTextColor(TFT_YELLOW);
}
else if (data1 < 151){
tft.setTextColor(TFT_ORANGE);
}
else {
tft.setTextColor(TFT_RED);
}
tft.setFreeFont(FF18);
tft.drawString("AQI",250,78);
}
}
//connect to mqtt broker on JEDI One and subscribe to topics
void reconnect() {
// Loop until we're reconnected
while (!client.connected()) {
Serial.print("Attempting MQTT connection...");
// Create a unique client ID using the Wio Terminal MAC address
String MACadd = WiFi.macAddress();
MACadd = "WioTerminal" + MACadd;
String clientID = MACadd;
// Attempt to connect
if (client.connect(clientID.c_str())) {
Serial.println("connected");
// set up MQTT topic subscription note: topic needs to be "datacache/" + Device on JEDI One
Serial.println("subscribing to topics:");
//Serial.println(subtopic1); //comment out subtopic1 for this revision of code
//client.subscribe(subtopic1);
Serial.println(subtopic2);
client.subscribe(subtopic2);
Serial.println(subtopic3);
client.subscribe(subtopic3);
} else {
Serial.print("failed, rc=");
Serial.print(client.state());
Serial.println(" try again in 5 seconds");
// Wait 5 seconds before retrying
delay(5000);
}
}
}
void setup() {
// setup lcd display
tft.begin();
tft.setRotation(3);
tft.fillScreen(TFT_WHITE); //Black background
spr.createSprite(320,110); //try 320x110
tft.setFreeFont(FF19); //select font
tft.setTextColor(TFT_BLACK );
tft.drawString("Outdoor Air ",5,5);
tft.drawString("Quality",195,5);
tft.setTextColor(TFT_BLACK);
tft.setFreeFont(FF18);
tft.drawString(" Ozone AQI: Particle AQI:",10,50);
tft.drawString(stamp,60,110);
tft.setFreeFont(FF18);
tft.setTextColor(TFT_BLACK);
tft.drawString("AQI",250,78);
tft.drawString("AQI",100,78);
tft.fillRect(0, 40, 320, 2, TFT_BLACK);
Serial.begin(115200);
setup_wifi();
client.setServer(mqttServer, 1883); //set mqtt server
client.setCallback(callback);
}
Main loop checks if connected, checks for MQTT messages and pushes latest line chart of sensor data to the LCD display
void loop() {
// check if connected to mqtt
if (!client.connected()) {
reconnect();
}
if (msg == 1) { // check if new callback message
msg = 0; // reset message flag
Serial.print("decoded timestamp = ");
Serial.println(stamp);
Serial.print("decoded data1 = ");
Serial.println(data1);
Serial.print("decoded data2 = ");
Serial.println(data2);
// update line chart code
// chart consists of two lines tracking values data1 and data2
Serial.print("data[].size = ");
Serial.println(data[0].size()); //debug - print data[] size for line chart
if (data[0].size() == max_size) {
for (uint8_t i = 0; i<2; i++){
data[i].pop(); //this is used to remove the first read variable when max_size reached
}
}
data[0].push(1.0 * data1); //read variables and store in line chart data array
data[1].push(1.0 * data2);
// Serial.println(data[0]); //debug
spr.fillSprite(TFT_WHITE); //clear line chart area
//Settings for the line graph title
auto header = text( 0, 100)
.value("test")
.align(center)
.valign(vcenter)
.width(tft.width())
.thickness(3);
header.height(header.font_height() );
// header.draw(); //Header is not used so disabled
auto content = line_chart(20, header.height()-10); //(x,y) where the line graph begins
content
.height(tft.height() - 140) //header.height() * 1.5) //actual height of the line chart
.width(tft.width() - 20) //actual width of the line chart
.based_on(0.0) //Starting point of y-axis, must be a float
.show_circle(false) //drawing a cirle at each point, default is on so set to false.
.value({data[0], data[1]}) //passing through the data to line graph
.color(TFT_PURPLE, TFT_BLUE) //Setting the color for each line
.draw();
spr.pushSprite(0, 130); //display line chart
}
Serial.println("debug - in main loop");
delay(2000);
client.loop();
}
4 - Example Serial Monitor output from Arduino code
Various Print statements have been inserted in the example Arduino code to help during debug and code modifications. Example output is shown below.
5 - Latest source code for the WioTerminalMQTTDisplay2topicOAQrev2.ino application is on github at below link:
Set up the JEDI One
1 - If machinechat JEDI One is not already installed on the Raspberry Pi see below:
- Get Raspberry Pi version of JEDI One DK-JEDIONE-RP
- Install on Pi, see Raspberry Pi - Installing JEDI One as a Service
2 - Set up the JEDI One as described in the referenced two projects First project is Machinechat with Renesas ZMOD4510 Outdoor Air Quality Sensor. Second project is Machinechat with Panasonic SN-GCJA5 Air Quality (PM) Sensor.
Example JEDI One air quality data screenshot.
Conclusion
Seeed’s Wio Terminal makes it easy to implement a low cost full color graphical remote MQTT data display for outdoor air quality. It’s built-in WiFi and associated Arduino libraries enable a direct connection to the JEDI One MQTT broker running on the Raspberry Pi. Machinechat’s JEDI One IoT data management provides MQTT access to any data it is collecting as well as additional processing, alerts or other actions.
References
- Seeed - Wio Terminal Product Page
- Seeed - Wio Terminal Wiki
- Seeed - Wio Terminal LCD Linecharts
- Seeed - Wio Terminal LCD Fonts
- Getting Started with machinechat’s JEDI One IoT Platform
- Arduino - How to use ArduinoJson with PubSubClient?
- machinechat Product Guide - Built In MQTT Broker - Data Collector
- machinechat Product Guide - MQTT Broker - Subscribing to a topic
- HIVEMQ - MQTT Essentials
- EPA - Ground-level Ozone Pollution website
- EPA - Particulate Matter (PM) Pollution website