Hello,
I am looking for Smallest Bidirectional Level Translator/Shifter(BGA,X2SON package) with Smallest Foot Print for i2C and GPIO level shifting.(3.3 v to 1.8 v)
It should fit in 1.2 mm X 2 mm .
Any ideas , I have searched a lot on various places with no luck.
Regards,
S
smallest i could find is 1.9 mm X 1.4 mm : link
Hello,
Welcome to the Digikey tech forum. I found these options searching by package size only.
Thanks ! but apart from smallest package total number of outputs should be at least four.
Does x - bit means x outputs?
we need 4 bit at least for 4 signals. Sadly cant apply this filter.
found this : Dual bidirectional I3C/I2C-bus and SPI voltage-level translator (nxp.com) but it is 2 bit
Any comments?
Regards,
S
See if this one will work for you:
PI4ULS3V204GAEX Diodes Incorporated | Integrated Circuits (ICs) | DigiKey
Package: 12-CSP (1.37x1.87)
Thanks this 12 pin looks good. Checking it.
Regards,
S
Yep, the only ones I found nearly that size were the LSF0204xYZPR in the 1.9mm x 1.4mm 12-DSBGA package and the PI4ULS3V204GAEX Kristof pointed out.
Yes it suits for i2c . Hope it suits for gpio as well though it doesn’t mentions that fit
Regards
S