SMD 5 Pin Regulator

Hello,
Actually this IC located in board related to Honeywell IP camera model: H3W2GR1.
when test the IC the voltages will be as illustrated in below picture:
1704995855402-2

The problem in the board in general that the power did not reach 3W to all the camera connected with the host, the power reach only 1.6w only while in the working probably camera the power reach 3w then 5w

I don’t know if this IC caused this fault or no since I didn’t recognize it