Hi,
What is the different between SMF5.0AHRVG and SMF5.0AH?
MFG: Taiwan Semiconductor
Hi,
What is the different between SMF5.0AHRVG and SMF5.0AH?
MFG: Taiwan Semiconductor
Hello,
Welcome to the TechForum!
Here is what I was able to confirm: the SMF5.0AHRVG and SMF5.0AH are the same part other than how it is packaged and received. 2 different heat temps that change the package cases.
The SMF5.0AH parts are the same part. When the ending is changes after the AH it indicates the packaginf type, 7" or 13" reels, 2,34 and 10k-20k qty options as well.
AH will indicate industrial temps -55°C ~ 175°C (TJ) and package case SOD-123W
Non AH will be standard operating temps -55°C ~ 150°C (TJ) package case SOD-123FL
Please let us know if you need any more assistance.
Thank you
Ryan