------Question for CR102J3RS215QF7 Please Put your question below------
Hello greggk47,
Welcome to the DigiKey TechForum.
As Paul said, this CR102J3RS215QF7 is a basic ON-OFF single pole single throw switch.
Regards.
My inquiry is, will the switch light up when turned on? I previously bought a switch on PO REDACTED, and when I installed and turned it on, the switch lit up momentarily, then the light burned out. I’m using it on a 120V power source.
The typical cause of this behavior is a failure to note that the illumination voltage and rated contact voltage often differ. A switch such as P/N CW103-ND for example can be used to switch 120VAC, but the illumination source is designed for 12VDC.
P/N CR102J3RS215QF7 by comparison indicates a nominal illumination voltage of 125VAC.