Switch stroke 800SP9B5M1QEH

------Question for 800SP9B5M1QEH Please Put your question below------

Can you tell me the stroke of this switch for actuation as I can’t see this on the data sheet

Hi @paul.johnson ,

Welcome to DigiKey TechForum and thanks for your inquiry.

According to the drawing, this switch has two dimensions, corresponding to the off position and the on position respectively.

image

Hi Thanks for the reply. I was reading the drawing as the main body being 5.59 and the switch button as 3.94. These dimensions correspond to the 3D CAD. However it doesn’t show the dimension of the compressed button position ie the travel of the switch. Could you let me know of the travel the button will depress by ie the travel.

Thanks

Hello,
I wasn’t able to find the travel dimension, I’ll put in a request to see if this information is available and post when I get it.

Thank you for the information and the help. I really appreciate it

The total travel for this is 0.8 to 1.0 mm.

Hi thanks for the information. Is there a switch like this one with 1.5-2mm travel

Hello paul.johnson,

Unfortunately, while trying to keep the specifications as close to 800SP9B5M1QEH as I can, I do not see that we have an option with the requested travel range.

Thank you for the clarification