Hi,
I’m looking for a terminal block (for 18 AWG Hook-Up Wire) which has a metal cover. A plastic cover is also acceptable, but then it needs to be UL certifified with 5V Flammability rating. Do you have this in stock?
We use it for a ventilation system which uses 50Watt at max. The fans are 230V. There is a trafo (230v to 115v) installed so it can be used in the United States. The trafo is connected on one side of the terminal block and the cable to the power outlet on the other side. Do you have this or something similar in stock?